Feedback_Position_Error_Limit

 Feedback_Position_Error_Limit

Address: 10248 (2808H)
Type: Unsigned32
Access: Read/Write
Unit: IU (one motor turn = 65536 IU)
Range: Unsigned32
Default Value: 10000
Store Supported: Yes
Description: This value is used for Feedback feature and define the maximum allowed displacement between motor ref position and motor actual position detected by encoder. When the displacement limit is reached, the motor is stopped depending by object Feedback_Settings.Type,
Notes: See Closed Loop Modality for details.